Issue:
Wanting to know if he could use SoMove V2.2, with Windows 8?
Product Line:
ATV32 , ATV61, ATV312, ATV212, ATV71, ATV12
Environment:
All
Cause:
Installation / Setup
Resolution:
Yes SoMove v2.2 is compatible with Windows 8 (and 8.1).
SoMove V2.2 has been obsoleted...current version (as of April 2017) is V2.6
Wanting to know if he could use SoMove V2.2, with Windows 8?
Product Line:
ATV32 , ATV61, ATV312, ATV212, ATV71, ATV12
Environment:
All
Cause:
Installation / Setup
Resolution:
Yes SoMove v2.2 is compatible with Windows 8 (and 8.1).
SoMove V2.2 has been obsoleted...current version (as of April 2017) is V2.6
Released for:Schneider Electric Egypt and North East Africa