Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will an External Fault triggered by a logic input be recorded in the fault history on an ATV61 / ATV71 series drive?
Issue:
Does an External Fault triggered by a logic input get recorded in the fault history?

Product Line:
ATV61 / ATV71 series drives

Environment
All models, All serial numbers

Cause
Customer needs a fault history on how many times an external fault is triggered.

Resolution:
An external fault triggered by a logic input will be recorded into the fault history and can be retrieved by navigating to the diagnostics menu and entering the fault history sub-menu.