Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the retrofit kit options to replace a CM2000?

Issue
The customer wants to replace a CM2000 with another Powerlogic meter.

Product Line
CM2000 Series Meter, PM8000 Series Meter, PM5000 Series Meter

Environment
Hardware installation, Adapter Plate

Cause
Require a retrofit solution or bracket for CM2000 replacement.

Resolution
Below are the options available as of August 2016.

Retrofit Assembly Options

  • CM2TOPM8K
    • CM2000 to METSEPM8244 remote display meter retrofit assembly. Includes meter and assembly fully pre-wired for direct CM2 replacement.
  • CM2TOPM5K
    • CM2000 to METSEPM5563RD remote display meter retrofit assembly.  Includes meter and assembly fully pre-wired for direct CM2 replacement.


Bracket Only Options

  • APPMCM2
    • PM integrated display mounting adapter for CM2000 replacement.

For an example of the submittal drawings please see FA314511 . These drawings are the same for both the PM8000 and PM5000 series.

Note:
CM2TOPM800 Retrofit Kit is no longer available - if this is an integrated display, the alternative is to use the APPMCM2 bracket as PM8K 96x96mm dimensions are the same as the PM800 series.

Obsolescence:

  • CM2TOION7650
    • CM2000 to ION7650 (S7650A0C0B6A0A0A) integrated display meter retrofit assembly (not available since 8/1/2019 as ION7650 series meters are obsolete).
  • CM4MA
    • CM4000 mounting bracket or CM2000 replacement (not available since 12/31/2019 as CM4000 series and accessories are obsolete).