Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does Graded Insulation mean in Medium Power Transformers?
Primary side star connected transformers may have a graded insulation on their neutral point in order to optimize the design of the bushing & winding configuration. Due to the electrical characteristic of the neutral point, the Lightning Impulse withstand voltage levels can be graded compared to the primary phases. Thus, we can choose a lower insulated bushing and can design the winding accordingly. This will optimize the overall transformer design. However, this point needs to be agreed with the customer in any case.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center