Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the reaction of the product when devices as WIFI are emitting under 2,4GHz
Because with the frequency hopping given by our protocol we avoid there pollution. The complete design of eXLhoist was done with a Wi-Fi station at 1,5 m from the systems. No perturbation was identified.