Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you set up the ATV12 drive to start and stop with terminal inputs and use the local knob as speed control?
Issue:
ATV12 set up to start and stop with terminals and use the local knob as speed control

Product Line:
Altivar 12, ATV12, Machine Drive

Resolution:
Programming
1st put the drive in local control mode by holding the MOD button for 3 seconds. 3 leds on the display are flashing one two three one two three.
2nd once you are in local mode you will now need to hold down ESC for 3 seconds to get the drive into a local programming mode. 3 leds are now flashing all three at once.
now you can program the drive.
With the drive in a RDY state,  Push enter and scroll down to ConF enter
scroll down and find FULL enter
scroll down find CTL menu enter
Fr1= A1U1 enter
CHCF= SEP enter
CD1= term enter
Hold the ESC button for 3 seconds until the  three Leds are flashing one two three again

Now LI1 is start for 2 wire control and the local knob will be the speed control.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa