Issue:
Setting ATV212 for Automatic Restart after a power outage, when the drive is in local control mode.
Product Line:
Altivar ATV212 S-flex Sflex 212 Sflex 21
Environment:
All
Cause:
The drive is not restarting in after a power outage while running in local mode.
Resolution:
The drive will not reset after a power outage when it's in local mode. You will need to push the Run button again to start the drive.
If you want an automatic restart after a power outage, consider using a 2-wire dry contact for starting on the terminal inputs.
Released for: Schneider Electric Egypt and North East Africa