Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why is command switching not visible on the ATV71?
Issue:
Command switching is not visible on the ATV71.

Product Line:
Altivar 61, Altivar 71

Environment:
All serial numbers, all model numbers

Cause:
N/A

Resolution:
On the ATV61 or the ATV71, command switching will not be visible if profile is "not separate".   Profile set to "not separate" means the command comes from the same place as the reference.

Schneider Electric Egypt and North East Africa