Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to read the IP address of a High end M580 CPU
Issue

Where is the M580 IP address located?

Product Line

BMEP585040, BMEP586040
Unity pro 11 and above.

Resolution

The IP address is located in two system words: %SW6 and %SW7.

%SW6 contains the two last octets of the IP address and %SW7 contains the two first octets.

Schneider Electric Egypt and North East Africa