Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the current replacement for the ConneXium 499NSS25102 switch?
The ConneXium switch part#499NSS25102 has 3 10BASE-T copper ports and 2 100BASE-FX single mode fiber ports. So the closest replacements to this switch would be the ConneXium Part#TCSESM043F2CS0 (2- 10/100BASE-TX copper ports and 2- 100BASE-FX single mode fiber ports) or the ConneXium Part# TCSESM083F2CS0 (6 10/100BASE-TX copper ports and 2 100BASE-FX single mode fiber ports) switches..

Schneider Electric Egypt and North East Africa