Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the phase loss protection on the ATS48 soft starter be turned off?
Issue:
Can I turn off the phase loss protection on the ATS48?

Product Line:
ATS48

Environment:
All model number, all serial numbers

Cause:
N/A

Resolution:
No, the PHF cannot be turned off. Parameter PHL (Phase Loss Threshold) can be adjusted between 5% or 10%.