How can we help you today?

iRIO Modbus Function Code 02, is iRIO able to read Modbus finction code 02 (input status) ?

Yes, it's possible to  configure the modbus function code 02 need  to be configured in the variable address field

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center