Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can an external 24VDC source be used to control an ATS48 softstart?
Issue:
ATS48 softstart controlled by an external 24VDC source

Product Line:
Altistart 48, ATS48

Environment:
All

Cause:
N/A

Resolution:
Yes. The logic inputs will work with the internal or an external power supply. If an external +24 DC source is used, connect the power supply common (-) to the ATS48 COM terminal, giving them a common reference point.

Schneider Electric Egypt and North East Africa