Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Cannot change the FTP password for the TSXWMY100 using Web Designer.

Issue
Cannot change the FTP password for the  TSXWMY100 using Web Designer.

Product Line
Ethernet Module Premium

Environment
TSXWMY100

Resolution
The selection for FTP password on the target security window is greyed out and not selectable.
image1


Due to cyber security reasons, the ability to change the FTP password for TSXWMY100 Factorycast HMI module using
Web Designer is not allowed.   Changing of the FTP password for the  TSXWMY100 Factorycast HMI module must be
performed from the 'Setup' web pages.