Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to command the Altivar VFD to do a ramp stop via Modbus serial communication?

Article available in these languages: Spanish

Issue:
Altivar VFD ramp stop command via Modbus serial communication

Product Line:
ATV31, ATV312, ATV61, ATV71, ATV58, ATV12, ATV32

Environment:
All serial number

Cause:
N/A

Resolution:
To command the VFD to do a ramp stop, a decimal value of 7 must be written to the command word.