How can we help you today?

How to wire properly the positive/negative signal to D0/D1 pin of serial port on M340 or NOM for RS485

Question:
How to wire properly the positive/negative signal to D0/D1 pin of serial port on M340 or NOM for RS485?


Answer:
RS485 is the difference signal, so it makes no sense to indicate positive / negative for D1, D0.
Due to the different convention, customer may came across Data+/Data- or B/A combination of wires.
Just wire the Data+ to D1 or B to D1, remeber that when D1>D0, the logical signal is positive inside while it is negative when D1<D0

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
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
Start your sales enquiry online and an expert will connect with you.
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
  • Help and Contact Center