Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I configure an M580 PAC to log events to a syslog Server?
Goals and Symptoms
Syslog is a standard messaging service that can be used to monitor security and other events. It is available on the M580 using
Unity Pro version 10.0 or greater. The attached document  is a descriptive example of using syslog with Unity.

Facts and Changes
In a system using syslog the M580 acts as a client sending messages to a syslog server. Each message is time-stamped
and an NTP or SNTP server must also be configured. This example uses a BME P58 1020 PAC. The NTP server is a
TCSESM083F2CU0 Connexium switch. The syslog server is an open source server Visual Syslog. The configuration of each is
described in the attachment.

Schneider Electric Egypt and North East Africa

Attachment(s)
SYSLOG .pdf [1.09 MB]