Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you use the Lonworks card from an ATV21 on an ATV212 and vice versa?
Issue:
Usage of a Lonworks card from an ATV21 on an ATV212 and vice versa

Product Line:
Altivar 21, Altivar 212

Environment:
All

Cause:
N/A

Resolution:
No.
The ATV21 drive's lonworks card part number is VW3A21312.
The ATV212 drive's lonworks card part number is VW3A21212.