Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: Adding a device profile to an AS-i configuration using Ecostruxure Control Expert (formally Unity Pro).
Issue:
How do you add a device profile in the AS-i configuration using EcoStruxure Control Expert ( formally Unity Pro)?

Product Line:
AS-i, Quantum , Premium

Environment:
Ecostruxure Control Expert ( formally Unity Pro)

Cause:
Unable to create the profile into the software.

Resolution:


Schneider Electric Egypt and North East Africa