Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the ATV212 Bacnet terminals isolated from the drive controls?
Issue:
Bacnet terminals isolated on the ATV212.

Product line:
ATV212, Altivar 212

Environment:
all

Cause:
Customer is concerned about grounding on the bacnet card and the other drive terminals that may cause noise.

Resolution:
SCR:
- is isolated from drive's ground (chassis)
- is isolated from any other drive's terminals
GND:
- is isolated from drive's ground
- is connected to CC terminals
- is isolated from any drive's Earth