How can we help you today?

Unity Pro crashed when loading a CNF file inside a TSXPBY100?

When the CNF file is loading inside the TSXPBY100, UPV10 crashed.
This is also true with Unity Pro V8.0, V8.1 and whatever the Sycon version used to build the CNF file.

A TSXPBY100 has 8 KWords of memory. Profibus slave consumes Bytes of configuration. Main parts of these Bytes are linked to the ‘Max_User_Prm_Data_Len’ parameter. The master also uses some configuration words. This crash occurs when the TSXPBY100 memory is over reached.
[((8*1024)*2)/(Slave configuration bytes)]+ master = MAX slave number

‘Max_User_Prm_Data_Len’ parameter size can be found inside the device DFB.

A Unity Pro V11.1 Hot Fix will be done for 2Q2016 in order to avoid that Unity Pro be closed. Instead of a message will pop up when this limit will be reached.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center