Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
BMXART0814 appears to be consuming two additional registers.
Issue
BMXART0814 appears to be consuming two additional registers.

Product Line
BMXART0814

Environment
Unity, Control Expert

Resolution
If you configure a BMXART0814 and an analog module (e.g., BMXAMI0810) with no gap in the state ram assignment between the
two modules, the first two registers of the analog will appear not to work or overwritten.

The reason this occurs is because the BMXART0814 reserves two additional registers for the cold junction.

The workaround is to allocate a two register gap between the two modules.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center