Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why is ENM8.3 not filtering low priority tags from PME8 system

Issue

Why is ENM8.3 not filtering low priority tags from PME8 system

Product Line
Power Monitoring Expert 8.x
ENM v8.3

Environment
ENM Configuration

Cause
Alarm Configurator in PME is used to build various alarm rules by assigning priorities 100 and higher. ENM configuration of the PME alarms are working as expected; however, meter events from PME with priorities as low as 10 are being sent out to the subscriptions recipients.

Resolution
In ENM Configuration, select Subscriptions Recipients and confirm which Tag Filter is selected. ENM by defaul,t has all low priority and high priority events from PME. If the Tag Filter "All" is selected in the subscription, then all events will be sent out to the subscription's recipients.


ENM Subscription 1

ENM Subscription 2



ENM Subscription 3

For each subscription recipient, build the subscription by using the Add Subscription for each Tag filter in the system, except the tag filter "All"

NOTE: Starting in PME2020, the ENM function has been embedded within the PME web application https://www.se.com/us/en/faqs/FA403988/

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center