How to connect the TSXNTP100 to 140ERT85420 for clock synchronization
Some user can't find the diagram of the connection guidle for TSXNTP100 and 140ERT85420. Some can find the data sheet of NTP100 but it is failure with the clock synchronization.
please refer to this notes for them. which had been verificated in lab.
I get the pin of RJ45 for RS485 of TSXNTP100 from R&D. you should connect the PIN5(RJ45) to PIN38(ERT), PIN4(RJ45) to PIN40(ERT).
There is a mistake of the doc, you should exchange the PIN4 and PIN5
please refer to this notes for them. which had been verificated in lab.
I get the pin of RJ45 for RS485 of TSXNTP100 from R&D. you should connect the PIN5(RJ45) to PIN38(ERT), PIN4(RJ45) to PIN40(ERT).
There is a mistake of the doc, you should exchange the PIN4 and PIN5
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.