How can we help you today?

To configure a Profibus Remote Master with a M580 PLC range, a channel number must be define. The help of UnityPro doesn't deliver the channel number for a M580 PLC range. => Which channel to select?

If the PRM (Profibus Remote Master) is configured as a DIO in a M580 PLC, the channel number "03" must be configured in the PRM management Function Bloc.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center