Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What Values are Stored in the Primary, Secondary and Tertiary Registers for each Accutech Wireless Field Unit Type?

Accutech wireless field units have registers for Primary, Secondary and Tertiary process values. Please note that not all field unit types use all three process output values.


In general, the units for each field unit are fixed, despite the fact that you can change the units being displayed on the field unit display or in Accutech Manager. The exceptions to this are the DP10/DP20, the GL10 and the SL10, which can be used to measure different values such as Flow, Level or Pressure.

Schneider Electric Egypt and North East Africa