Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
User lost the username and password to the BMENOC0311 module.
Issue
The user lost the username  and password to access the HTTP web page in the BMENOC0311 module and needs to
reset it back to the default setting.

Product Line
Ethernet Module M580

Environment
BMENOC0311

Resolution
Due to cyber security reasons, the database that holds the username and password for the HTTP website on the module
is stored in a special chip on the board in the module.  It is not accessible using either Web or FTP access  The database
can only be accessed through a special hardware device that must be physically attached to the interface on the board.

The user must send the module back to the factory for a repair in order to reset the username and password back to
the default setting.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center