Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the value of "Control Effort" indicate in an Altivar drive being controlled via CanOpen?
Issue:
Altivar drive controlled via CanOpen indicates "Control Effort" value.

Product Line:
All Altivar drives equipped with CanOpen communication

Environment:
All Altivar drives controlled via CanOpen

Cause:
Information not clear in current literature.

Resolution:
"Control Effort" is an indication of the current actual speed of the motor and is a 32 bit unsigned integer.