Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Geo SCADA: Licensing a ViewX client with a license file

Problem

This article explains how to match up and install a ViewX license file in the associated ViewX client PC.

Solution

1) Open the license file using Windows Notepad.  You should see something like the screen shot below (note the 'MachineID' string)

image1

2) On the ViewX client PC click on the Windows Start button and navigate to EcoStruxure Geo SCADA | Configure Connections.  The Geo SCADA Client dialog should open as shown below.


image2

3) Click the 'Licenses' button (circled in red above).  The 'Client Licensing' dialog should appear as shown below.  Look at the Machine ID field.


image3

4) The machine ID in this dialog should match the machine ID shown in the license file.  If they do not match, you will need to check if another license file is available until you find the one that matches.  Once you find the matching license file click on the box with the 3 dots next to the license file field (as shown below)


image4

5) Navigate to the location of the license file and then click the 'Open' button

Note: it is recommended that users save the license file to folder C:\Program Files\Schneider Electric\ClearSCADA.  If the license file is saved in too deep a path (in the Windows directory), the Geo SCADA License Server may not recognize the license file.

image5

6) If the license installation was successful the 'License Mode' field should read "File based client license" and the 'Validity' field should read "Valid"
(Note: you may need to hit either the 'Apply' or 'Refresh' button first)


image6

7) Repeat these steps above for any other ViewX clients until all have been successfully licensed.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center