Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In Sepam, is it possible to customize the labels of the data in the disturbance recording?
Yes, it is possible to change the labeling of the data in the disturbance recording. Unfortunately, you need to do it every time the disturbance recording is being viewed in SFT2826 or other tool. The automatic customization of the labeling is not possible because the labels are embedded in the Sepam itself.

Schneider Electric Egypt and North East Africa