How can we help you today?

Geo SCADA Database Restore

Problem

How do I properly restore a Geo SCADA database?

Solution 1

Starting with ClearSCADA 2015, Geo SCADA features a 'Backup' object.  If a 'Backup' object was used to backup the database, follow the procedure in the ViewX help to restore the database.  The procedure may be found here:

ViewX Help | System Administration | Server Administration | Back up the Database | Load your Backup Database Files

Solution 2

Follow the steps below to restore a Geo SCADA database that was saved manually.

1) Open a Windows Explorer dialog and locate the 'Database' folder.  On a Windows 10 PC the location should be

C:\ProgramData\Schneider Electric\ClearSCADA\Database

database location

(The Database location may be found by right-clicking on the server icon, selecting ‘Configuration’ and then navigating to System Configuration | Location.

All fields should be common to a folder named ‘Database’)


server configuration


2) Bring the Geo SCADA server icon into view by selecting it from the system tray.


server icon 1


3) Right-click on the server icon and select ‘Shutdown Server’. NOTE: Never copy or replace a database while the Geo SCADA server is running.  The database could be corrupted if the server is not shut down first.



server icon shutdown


4) Wait for the server icon to first turn red (shutting down) and then grey.  When the icon turns grey, the Geo SCADA server has been fully shut down.



server icon 2

5) If you are restoring a database from the same folder directory then use the following procedure.  (If you are restoring a database that is stored in another directory/media location then you will need to switch between Windows Explorer dialogs.)

After ensuring that the server is shut down, rename or delete the ‘Database’ folder.


database folder 5


6) After deleting the ‘Database’ folder you should be left with the database folder that you wish to restore.   (If the database you wish to restore is stored elsewhere, move it to this directory.)


database folder 2


7) Rename the folder to the name ‘Database’.


database folder 3


database folder 4


8) Start the Geo SCADA database, open ViewX and the new Database will be presented.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center