Issue
Unable to print subscription reports from PME/Web Applications/Reports even when it says it was successful.
If the report is saved to the desktop, it prints OK.
From the Desktop works because it is using Windows not PME.
Product Line
All versions of Power Monitoring Expert (PME)
Environment
Power Monitoring Expert
Printing Reports
Cause
The installed printer does not allow printing from subscription reports in PME/Web Applications/Reports.
Resolution
In order to print pdf subscription reports, a TRUE PDF printer needs to be installed.
The printer specifications needs to include PDF under the Page Description Languages as shown below.
Page Description Languages (PDL)
PCL® 5c, PCL® 6, PDF direct, PostScript 3 compatible
Unable to print subscription reports from PME/Web Applications/Reports even when it says it was successful.
If the report is saved to the desktop, it prints OK.
From the Desktop works because it is using Windows not PME.
Product Line
All versions of Power Monitoring Expert (PME)
Environment
Power Monitoring Expert
Printing Reports
Cause
The installed printer does not allow printing from subscription reports in PME/Web Applications/Reports.
Resolution
In order to print pdf subscription reports, a TRUE PDF printer needs to be installed.
The printer specifications needs to include PDF under the Page Description Languages as shown below.
Page Description Languages (PDL)
PCL® 5c, PCL® 6, PDF direct, PostScript 3 compatible
Released for: Schneider Electric Egypt and North East Africa