Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why would a drive not stop when the run command is removed?
Issue:
The drive does not stop, when the run command is removed.

Product Line:
Altivar 61, Altivar 71, Altivar 312, Altivar 212, Altivar12, Altivar 32

Environment:
All serial numbers

Cause:
The VFD is not responding to the stop command.

Resolution:
1).  Verify how the drive is receiving the stop command.
2).  Verify if the drive is programmed to get the stop command from that source.
3).  Verify the drive is not in local control.
4).  Check if the run signal is jumpered/bypassed
5).  Check to see if the motor is backfeeding voltage back into the drive.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center