{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to correctly derive the DOM (Date of Manufacturing) displayed on meter HMI .
PM51/53xx meters are provided with a feature by which user can select the Date format .Date/month and year. The Available options are MM/DD/YY, YY/MM/DD, DD/MM/YY.The format selection is accessible from
Set up -->HMI --> Regional Setting menu

The Date format is applicable for DOM as well as Time related parameters.

The meters produced till 31st Dec 2015, there is a conflict for the DOM displayed and the format selected. The actual relation for these are provided in the below table.
Format SelectedDOM displayed on HMI
MM/DD/YYYY/MM/DD
YY/MM/DDDD/YY/MM
DD/MM/YYMM/YY/DD

An example for DOM 28th Dec 2015  is illustrated below
Format SelectedDOM on HMIActual
MM/DD/YY15/12/2812/28/15
YY/MM/DD28/15/1215/12/28
DD/MM/YY12/15/2828/12/15

Note : The issue is been solved by correcting the production Tool. All meters manufactured from 7th Jan 2016 onwards will not have this issue and DOM will match with the Date format selected

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.