How can we help you today?

Does Sepam series 10 has a dedicated setting tool just like SFT2841 for Sepam 20, 40, 60, and 80?

Issue

A user wants to know whether the Sepam Series 10 has a dedicated configuration and setting software tool similar to SFT2841, which is used with other Sepam relay series.

Product

  • Sepam Series 10

Environment

  • Sepam Series 10 protection relays
  • Relay configuration and parameter setting activities
  • Engineering and maintenance environments

Cause

Users familiar with Sepam Series 20, 40, 60, and 80 may expect a dedicated software tool such as SFT2841 to be available for configuring and managing Sepam Series 10 devices.

Resolution

Sepam Series 10 does not have a dedicated setting tool equivalent to SFT2841.

Additionally:

  • SFT2841 is not compatible with Sepam Series 10.
  • The setting and configuration methods used for other Sepam series that support SFT2841 cannot be applied to Sepam Series 10 through this software.

Users should refer to the appropriate Sepam Series 10 documentation for available configuration and setup procedures.

Schneider Electric Egypt and North East Africa
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
  • Help and Contact Center