Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a conformal coating option for the HMIGTU series?
Yes, the Magelis HMIGTU series are available with conformal coating. Part numbers shown below:

HMIG3UFC Premium Box
HMIG5UFC Open Box

HMIDT351FC 7" Screen
HMIDT542FC 10.4" Screen
HMIDT551FC 10" Screen
HMIDT642FC 12.1" Screen
HMIDT651FC 12" Screen
HMIDT732FC 15" Screen

Schneider Electric Egypt and North East Africa