Issue
Can the 'sec_script_Security Editor1033.txt' file in the 'Unity\Security\Res\1033 folder be used to create security profiles?
Product Line
EcoStruxure Control Expert (formerly known as Unity Pro)
Environment
Windows 7 Professional, Unity Pro v10
Resolution
The 'sec_script_Security Editor1033.txt' file found in the in the 'Res\1033', 'Res\1031', 'Res\1034', 'Res\1036', 'Res\1040' and 'Res\2052' folders are used by the Security Editor and should not be touched. The files found in the folders are used for the language localization and are not meant to be modified by the user. Any attempts to modify these files could make Unity and the Security Editor inoperable.
The user must use the Security Editor to create the security profiles.
Can the 'sec_script_Security Editor1033.txt' file in the 'Unity\Security\Res\1033 folder be used to create security profiles?
Product Line
EcoStruxure Control Expert (formerly known as Unity Pro)
Environment
Windows 7 Professional, Unity Pro v10
Resolution
The 'sec_script_Security Editor1033.txt' file found in the in the 'Res\1033', 'Res\1031', 'Res\1034', 'Res\1036', 'Res\1040' and 'Res\2052' folders are used by the Security Editor and should not be touched. The files found in the folders are used for the language localization and are not meant to be modified by the user. Any attempts to modify these files could make Unity and the Security Editor inoperable.
The user must use the Security Editor to create the security profiles.
Released for: Schneider Electric Egypt and North East Africa