What is the direct PME web applications link to Dashboards, Alarms, Trends, Diagrams, Reports, or Tables
Product Line
Power Monitoring Expert 2023
Environment
Web Applications
Cause
By default, Web Applications opens in Dashboards but by using the links below, one can directly log into Alarms, Diagrams, Reports, Tables, or Trends.
Resolution
Before you attempt to create a link for your PME web application please see the notice below:
Use the integration utility settings to generate pre-authenticated links to PME resources. Use these links to integrate web applications (Dashboard, Diagrams, Trends, Alarms, Reports, and EWS measurements) into third-party systems. You can authenticate the link using standard users or Windows users.
As a precursor, please use the following steps to navigate to the Setting tab in the Web Applications
- Open Web Applications from the EcoStruxure Power Monitoring Expert folder on your desktop, the Schneider Electric folder on the Start Screen, or by entering the PME server URL into your browser Address bar, e.g.
http://srv1.MyCompany.com/Web - Open the Settings page from the SETTINGS link in the Web Applications banner.
To enable or disable the pre-authentication for standard users:
-
Under Pre-Authentication for Standard Users, turn Enable pre-authentication on or off.
-
Click Save to apply the changed settings.
To generate links:
- Under Authentication Method, select the desired user type for authentication:
- Select Windows User.
- Select Standard User, select the desired PME User Name and enter the Password.
-
Under Generate Links For, select the web applications for which you want to generate link.
-
Under Link Format, select the desired link format:
-
Select XML to generate an XML file of links. Use this option to generate links that can be imported into applications like EcoStruxure Building Operation.
-
Select HTML to generate an HTML page of links. Use this option to verify the links.
-
- Click Generate Web Application Links.
- An XML or HTML file is downloaded to the default download location of the browser.
An example for an application that requires the generated link is the integration of PME with Building Operation. As part of that integration, PME Web Applications are embedded in Building Operation. For this to work, the generated links are imported in to Building Operation.
Released for: Schneider Electric Egypt and North East Africa