Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you program the ATV312 drive to be controlled by the optional VW3A31101 remote keypad display?
Issue:
Programming the ATV312 drive to be controlled by the VW3A31101 remote keypad display.

Product Line:
Altivar

Environment:
All

Cause:
Wants to use the VW3A31101 remote keypad display for speed and start  stop control

Resolution:
Programming
RDY menu enter scroll down to CTL menu enter
CTL menu scroll down LAC make sure you are in L1 or level 1
CTL menu scroll down to LCC enter and set this to Yes.
LCC= Keypad control