Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I know if there is a broadcast storm on the network with an M580?
With Unity Pro V11, the BMENOC's DDT and the HSBY M580 CPU's DDT have a new attribute called "NETWORK_HEALTH" that helps diagnose if the network is ok. If NETWORK_HEALTH is false, this might come from an unintend loop resulting in a broadcast strom.
Most likely reason is that BMENOC Ethernet backplane ports are activated and a second RSTP loop is created.
Note that in BMENOC 03x1firmware version 2.04 and above, the Ethernet backplane port is disabled when the NOC is in the no_conf state. This prevents unintended loops when the NOC is not configured.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center