Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can an analog input be used for the PID reference with the Altivar Process Drive?
Issue:
Analog input usage for the PID reference with the Altivar Process Drive

Product Line:
ATV 600/900 series

Environment:
All models, All serial numbers

Cause:
Customer has an application with a dynamic setpoint and needs to use 4-20ma input for the PID reference.

Resolution:
Yes, If parameter PII (Internal PID Reference) is set to NO, the drive will use the Reference 1 channel as the PID reference. Reference 1 channel can be configured for any analog input.