Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the ATV630 (or ATV930) Process drive available with 1 phase input and 3 phase output?
Issue:
Are the Process drives available with single phase input and 3 phase output?

Product Line:
Altivar 630
Altivar 930

Environment:
Application

Cause:
Wants to know if the ATV630 Process drive is offered in 1 phase input 3 phase output.

Resolution:
The ATV630 is approved for some single phase input, 3 phase output applications.
See the current Annex to the Getting Started with Altivar Process ATV600 document below:
https://www.se.com/ww/en/download/document/EAV64300/

This document lists models for 240V and 480V Pump applications.
Note: Do not use ATV630D55M3 and ATV630D75M3 for 1-phase application.

At this time, no ATV900 Process drives are approved for single phase supply.  They are designed strictly for 3 phase input power to run a 3 phase motor.

The ATV900 series may be used in conjunction with a 3rd party input bridge from a company like Bonitron (Bonitron Solutions for Schneider Drives) .
Contact Bonitron directly for assistance.