Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the memory capacity for the EM4800 series onboard logs?
Issue:
A customer wants to know the maximum onboard memory capacity for one of the EM4800 series meters.

Product Line:
EM4800 series

Environment:
EM4800 series product line

Resolution:
The onboard logs for the EM4800 series are capable of holding up to 2.4 years worth of data when configured at a 1 hour logging interval or 219 days at 15 minute intervals.  The logging interval as well as the quantities to log can be configured through the EM4800 configuration utility.