Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the ATV Process drives (ATV630, ATV650, ATV930, ATV950) conformal coated? What about the ATV320 and ATV340?
Issue:
ATV Process and ATV Machine drives conformal coated.

Product Line:
ALTIVAR 630
ALTIVAR 650
ALTIVAR 930
ALTIVAR 950
ALTIVAR 320
ALTIVAR 340

Environment:
All

Cause:
N/A

Resolution:
Altivar Process (ATV6x0 and ATV9x) withstand to harsh environments:
- Chemical class 3C3 conforming to IEC/EN 60721-3-3.
- Mechanical class 3S3 conforming to IEC/EN 60721-3-3.
Except:
- Altivar Process ATV630C22...C31N4 drives are certified as chemical class 3C2 and mechanical class 3S2 conforming to IEC/EN 60721.
- Altivar Process ATV930C22...C31N4 drives are certified as chemical class 3C2 and mechanical class 3S2 conforming to IEC/EN 60721.

Altivar Machine (ATV320 and ATV340) withstand to harsh environments:
- Chemical class 3C3 conforming to IEC/EN 60721-3-3.
- Mechanical class 3S2 conforming to IEC/EN 60721-3-3.

However, in all cases, there are no published certificates that we can send out.