Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What will cause a CLr fault on the ATV212?
Issue:
Getting a CLr fault on the ATV212.

Product Line:
ALTIVAR 212

Environment:
All models

Cause:
Troubleshooting

Resolution:
CLr [Reset active] is a status which is displayed after the STOP/RESET key is pressed while a detected fault is displayed. It indicates that the cause of the detected fault has cleared and the fault status can be reset. Press the STOP/RESET key again to clear the detected fault.  This type of fault reset only applies when in Local mode or in Remote mode with CMOd=1 ( HMI ).  It also only applies to the following faults:
chart