Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the standard Burn-in process for ATV61/ATV71 drives?
Issue:
Standard burn in process for ATV61/ATV71 drives.

Product Line:
ATV61 ATV71

Environment:
All

Cause:
Additional Documentation Request

Resolution:
Manufacturing Quality Assurance Procedures for the Altivar 61 & Altivar 71 AC Drives
This document provides information regarding the quality assurance processes and procedures
that are in place for the manufacturing of Altivar 61 (ATV61) and Altivar 71 (ATV71) AC drives.
Schneider Electric utilizes quality assurance processes and procedures to verify the integrity of
components and the assembly process. Data is gathered on each unit and tracked via the
unique serial number of each unit. This document provides a summary of these processes and
procedures.

Schneider Electric Egypt and North East Africa

Attachment(s)
Quality_Assurance Customer Letter.pdf [54.42 KB]