M580 CPU : 2.13 or above
CRA : 2.16 or above
if older versions are used and the diagnostics EF is used for the CPS4002 (i.e. PWS_DIAG or PWS_CMD), then it may crash
Released for: Schneider Electric Egypt and North East Africa






Our Brands
Welcome to the Schneider Electric Website
CRA : 2.16 or above
if older versions are used and the diagnostics EF is used for the CPS4002 (i.e. PWS_DIAG or PWS_CMD), then it may crash
Discuss this topic with experts