Product Line:
M340, M580, X80
Environment:
Ecostruxure Control Expert
Resolution:
Unfortunately, you cannot;
The M340 and M580 ethernet ports can only send or receive Modbus TCP/IP or Ethernet/IP messaging. They cannot read or write in ASCII characters using these protocols.
The only option is to use the M340 Modbus serial port or BMX NOM 0200 module with the INPUT_CHAR or the PRINT_CHAR function blocks to read and write an ASCII string to or from a server device.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for: Schneider Electric Egypt and North East Africa