Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for a 30mm speed potentiometer to use with Altivar Drives?

Article available in these languages: Spanish

Issue:
Customer wants to use 30mm operators.

Product line:
Altivar

Environment:
all

Cause:
n/a

Resolution:
9001K2107 is a 5k ohm, 30mm speed potentiometer available from Schneider Electric. This includes the operator, speed pot and legend plate.
See attached screen shot for other options, but remember to confirm the allowable potentiometer range for the specific drive.



Schneider Electric Egypt and North East Africa

Attachment(s)
30mm potentiometer selection.PNG.png [57.36 KB]