Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What would cause the motor to jerk up and down when running an ATV312 drive?
Issue:
Motor jerking up and down when running an ATV312

Product Line:
Altivar ATV31 and ATV312

Environment:
All

Cause:
Motor is not running smooth its jerking back and forth.

Resolution:
Check the motor nameplate for the correct motor data.  Enter this data into the DRC and SET menu
DRC menu enter
BFr= 60hz
UNS= 230vac or 460vac motor voltage
FRS= 60hz
NCr= 2.4 amps  for whats stamped on the motor name plate
COS= .80
UFT= Change to L

SET menu
ACC= 1 to 10 seconds
DEC= 1 to 10 seconds
LSP=  Choose
HSP= Choose
ITh= 2.4 amps or whats stamped on the motor name plate
URF= 40%.